Seiko Instruments launches new Bluetooth USB Type-C POS printer model
Seiko Instruments is a leading expert in the upscale market segment of thermal printing technology. The wide range of Seiko Instruments also offers receipt and label printers for mobile applications for all printing requirements in everyday life, such as medical devices, self-service technology, at the POS and more. The key to success: high quality and reliability, advanced technology and quiet operation.
As the latest member of the RP-F10 POS printer series, Seiko Instruments launches the -5, a SEIKO RP-F10-K-3 equipped with a USB Type C port. It enables stable wired communication with Android/Windows/iOS/iPadOS smart devices as well as high-speed charging with support for USB Power Delivery (USB PD).
In addition to wired communication via USB, wireless communication via Bluetooth is also available, which enables high-speed charging via USB PD during wireless communication on Android and Windows. When using iOS / iPadOS (Lightning port), USB communication and charging with a maximum of 5V 2.4A are possible.
This will meet the increasing demand for host devices such as smartphones and tablets for mPOS applications, which must be supported by a high-speed charging function with USB-PD.
Other models of the RP-F10 POS printer series differ in interfaces. The -2 model offers the user a USB-A port, the -4 offers wireless communication via Bluetooth in addition to the USB-A port.
The new model is now available in our online shop. The other models from the series can be found here.