New rotating ball joint holder PRO HOLDER from Bernstein

Perfect holding device for cameras, monitors, sensors or measuring devices, the new ball joint holder PRO HOLDER from Bernstein can be used universally and configured individually. The ball joint can hold objects with a max. load of 140 kg and therefore it is also suitable for industrial use. This guide shows for which tasks the 360° ball joint holder PRO HOLDER can be used and its technical features, turning it into the perfect assistant. The new ball joint holder can be configured into the latest details. It is available in the online shop.

Strong holding power with precise clamping : Bernstein PRO HOLDER

Thanks to the ball joint, the strong holder can be turned in any direction and fixed in any desired position. The ball axis can be tilted by 45 degrees and rotated by 360 degrees. The maximum load capacity at the height of the threaded pin is 45 kilograms with a ball diameter of 40 millimeters. With a ball diameter of 60 millimeters, the highest possible load is even 140 kilograms. All equipment can be screwed on and ideally aligned via the thread on the ball. In addition to the model versions for clamping and screwing, the ball-jointed all-purpose holder is also available with a magnetic attachment.

This enables particularly flexible, ergonomic work, even on heavy parts, for example for repairing free-floating machines and for use in industrial metal and woodworking. This makes the new PRO HOLDER a valuable tool in industrial use, but it is also suitable for private use.

The ball joint holder for all cases

Compared to other systems already on the market, Bernstein’s flexible PRO HOLDER clamping and holding device impresses with its wide range of possible uses. While many holders available on the market are specialized for just one specific holding method, there are hardly any comparable models that have such universally applicable, rotatable ball joint holders as the new Bernstein PRO HOLDER.

Also in comparison to the often used but unsuitable mounting solutions such as converted monitor arms, camera tripods and the like, the robust PRO HOLDER from Bernstein convinces with its flexibility, durability and reliability.

In order to be able to hold heavy loads in any position, the articulated bracket is equipped with an external or internal thread. Bicycles, e-bikes and e-scooters can also be held freely with the help of the new PRO HOLDER, flexibly fixed and conveniently repaired – whether in the laboratory, in the workshop, in production or in the hobby room.

The universal mount in use

The movable clamping and holding device PRO HOLDER from Bernstein can be used in many different ways. In industrial electronics, for example, they fix infrared fire detectors in such a way that they can detect fires on conveyor belts or in battery storage facilities at an early stage.

In woodworking, the PRO HOLDER is used, for example, as a holder for a carving plate (carving ball). Different clamping and holding tools can be screwed on, making work easier. This combination is suitable for craftsmen in professional instrument making as well as model builders in the hobby workshop.

In the laboratory, at universities and in research centers, the universal holder with its versatile usage options has been valued for years.

Possible areas of application

Possible areas of application for the universal clamping and holding device include:

  • Presenting and repairing
  • Fastening and turning of bicycles, e-bikes and e-scooters
  • Attaching and rotating cameras, loudspeakers and sound equipment
  • Attachment and rotation of fire alarms, sensors and measuring devices
  • Operation of inspection and test stations
  • Movable instrument construction, for example violins and guitars
  • Woodworking, for example carving plates and balls
  • Model making, handicrafts and DIY

Quality made in Remscheid/Germany

Made in Remscheid has always stood for the highest standards of quality and origin of the raw materials for the specialist in the manufacture of ESD tools and ball joint vices. With many years of knowledge, products such as the new PRO HOLDER are processed into high-quality tools at the company headquarters in Bergisches Land.

Configure the PRO HOLDER individually

The new, individually configurable universal mount PRO HOLDER from Bernstein is available in its entirety in the online shop – freely configurable with all accessories and expansion components such as screws, table clamps and magnets. Depending on the application, you will find the right parts in the comprehensive range of different extensions, ball diameters and drives and outputs.

Images: Bernstein