Fishing like the pros – with the fishfinders from deeper
Fishing enjoys great popularity in Germany – whether from the shore or on a boat. With the fishfinders from deeper you can take your hobby to a new level: The combination of sonar technology and app helps you track down fish, giving you a fishing experience with a difference. This guide is designed to educate you on which fishfinder is the best fit for your interests.
Fishing with the Fish Deeper app
Even if fishing helps many people to switch off – a fishing trip also wants to be well planned. With the Fish Deeper app and a sonar fishfinder from deeper, you can plan your next trip ahead of time. Simply connect the sonar to the Fish Deeper app. Then download offline maps of the desired region to your smartphone and use them as a planning and orientation aid. Thanks to the app, you can also easily create depth maps of your favorite fishing spots – with an accuracy of 30 cm.
To launch the fishfinder, cast it similar to a fishing rod. The sonar device floats on the surface and uses echo sounders to scan the waters below. Now connect the fishfinder to your smartphone and you can use real-time scanning to check the condition and fish population of the body of water at your convenience. To do this, the Fish Deeper app gives you, among other things, the ability to adjust the scan angle or display sensitivity of your fishfinder to your liking with just a few clicks. If necessary, you can even display the depth at which fish of interest to you are swimming at the moment.

The fishfinders from deeper work like echo sounders. That is, they emit sound waves that bounce off objects they hit, such as fish, aquatic plants or the bottom of a body of water. The farther sound pulses radiate, the more likely they are to take on a cone shape. So a wide beam angle gives you a better view of a larger area. As a result, you miss fewer fish. Conversely, the beam cones also mean that a fish indicated on your phone may not necessarily be directly under your fishfinder. Rather, it may simply be swimming in the beam angle. Fishfinders with a GPS function, on the other hand, can show you their own distance to the fish you’re looking for, so you’re not fishing further in the dark.
The connection between the app and sonar fishfinder is via a stable Wifi connection. The fishfinder serves as a hotspot, so your phone does not need a network connection. So you can relax and concentrate on fishing without being disturbed. The app is compatible with both iOS and Android – and thus with most modern smartphones. In addition, deeper makes the app available through Huawei’s AppGallery, as well as the App Store and Google Store.
The deeper Start Fishfinder: Perfect for beginners
To familiarize yourself with deeper’s technology or if you are simply fishing from the shore, the deeper Start is the optimal entry-level model. Once cast into the water from the shore, you will be able to determine the vegetation of the water as well as the whereabouts of fish and thus the perfect fishing spot in no time. This leaves you with more time to spend fishing.
The deeper Start has a range of 50 meters and shows you results at depths between 50cm and 50m. Once connected to the app, the starter allows you to mark all interesting fishing spots on a map. If you’re planning a night fishing trip, you won’t lose sight of your fish finder thanks to the included automatic flashing light and you’ll know immediately where to cast your line.
Know where to go with your fishing rod – thanks to the deeper Smart Sonar PRO+ 2.
Planning a fishing trip from your boat – or even want to go ice fishing? Then the deeper Smart Sonar PRO+ 2 is the ideal fish finder for you. Thanks to improved GPS performance and three scanning beam frequencies, it allows you to scan up to 100m. This makes it the perfect companion for all experienced hobby anglers and professionals looking for a portable and versatile fishing gadget.
Easily create bathymetric maps from the shore as well as from the boat and get the distance of the fish finder to your smartphone thanks to the GPS technology. This way you know exactly how far to cast your fishing line. The different scanning frequencies allow you to scan larger areas. So, in the wide angle, you can scan the surrounding area for fish and in the medium scanning angle, you can examine the identified fishing spot. Then switch to the narrow angle to check the spot for surrounding fish.
The sonar update: the deeper Smart Sonar CHIRP+ 2
Excellent target separation and extreme depth accuracy at a range of up to 120m – the deeper Smart Sonar CHIRP+ 2 combines all this. This premium fish finder relies on the so-called CHIRP technology, which is an update to the sonar. True to its name Compressed High Intensity Radiated Pulse, a CHIRP sonar transmits a continuous frequency that ranges from low to high. A conventional sonar, on the other hand, only transmits single frequencies. This increases the clarity and accuracy of your data, and gives you much better resolution when viewing it on your smartphone.
Plus, thanks to CHIRP technology, noise and surface interference in the water are a thing of the past. Thanks to fast charging, you’ll also get the maximum battery life of 15 hours within just 120 minutes. Thanks to the included night fishing cover, there are no limits when planning your next fishing trip.
No matter if you go fishing at a lake only once a year or if you go on extensive fishing trips several times a year: The wide product portfolio of deeper offers the optimal additional equipment for everyone for the next fishing trip. Find the fishfinder that suits your needs in the reichelt online store now.

ctures: DEEPER