Wallbox made in Germany – the charging stations from LRT eMobility
The number of registered electric cars in Europe is steadily increasing. As a study by reichelt elektronik shows, almost two thirds of Europeans (69%) are considering buying an electric car. With the vehicle chargers (EVSE) from LRT eMobility, you can conveniently charge your electric car at home. The wallboxes from the German manufacturer are now available in the reichelt online shop.
A charging station for everyone – the Wallbox Essential
Driven by innovation and quality, LRT eMobility has set itself the task of making charging electric cars easier for everyone. The own division of LRT Automotive GmbH, a medium-sized production company near Heidelberg, places a special focus on private users. To be able to easily charge the electric car in your own garage, it doesn’t need a lot: a power connection and a wallbox. With the LRT E22 MFI of the Home Line Essential series, you can charge your car overnight without authentication. Thanks to the integrated, five-meter-long cable, you don’t even have to take the car’s cable out of the trunk. The charging station is available in the 11kW or 22kW version and, thanks to its IP44 certification, is ideal for both indoor and outdoor use.
In addition, you save real money in the long term with your own charging station: Compared to public charging stations, electricity is significantly cheaper – if you also use a photovoltaic system, you can feed in up to 100 percent of the electricity you need and charging does not cost you a cent. In addition, the purchase and installation of some wallboxes have been funded by KfW with up to € 900 since November 2020, including the LRT Car Chargers MFI.
However, please make sure during the installation that an electrician will lay the possibly necessary CEE sockets or cables. It would also be advisable to inform your network operator about your planning in order to cover your needs as best as possible.
E-mobility for the smart home with the Supreme line from LRT
The LRT eMobility product portfolio offers the perfect solution for every (smart) home. The best example of this is the Home Line Essential 11 KW: It is not only eligible for funding from KfW – thanks to the option of connecting it to your private WLAN via WiFi, it can be easily integrated into your own smart home.
The LRT Wallbox Home Supreme includes the same specifications as the Essential line, but it also has the advantage that you can easily authenticate yourself to your Ebox with RFID, PLC or app for charging and thus ensure that only authorized access to your Have a wallbox.
Billing individually and very easy to use – the charging stations of the LRT Business Line
With the solutions for business customers, LRT also has a wide range of wallboxes in the commercial sector. With a customizable accounting system and a wide range of functions for management and control via a web-based management system, the Business Line offers the perfect setting for every business customer.
The LRT BE22 MFI, for example, is an entry-level model: It can be connected to the WLAN via WiFi and thus integrated into a smart network. In addition, a funding application can be submitted to KfW for purchases and installations. With the user-friendly app, everyone can use the wallbox with ease – and thanks to the billing system with the eGiro function, you can ensure seamless usage billing.
With the LRT BE22 MFI, LRT eMobility has the supreme solution for your business in its range: Like the Essential model, this charging station is also eligible for KfW funding. Thanks to an integrated 4G module, however, you do not have to be close to your WLAN, but can instead enable your customers to charge their own electric car anywhere. As with the Essential model, you can use an RFID reader to ensure that only authorized end users use your charging stations. Thanks to the conformity with calibration law, billing to the cent is guaranteed at all times.
Regardless of whether you want to charge your electric car at home or are looking for the ideal solution for your business, employees and customers, the LRT eMobility charging stations leave nothing to be desired. The wall boxes can be easily integrated into the smart home or offer a customizable billing system – and all of this is “Made in Germany”. The broad product portfolio of LRT eMobility is now available in the reichelt online shop.
Image: LRT Automotive GmbH