Fischer EasyHook: Turn the screw into a hook
Conventional screw hooks are used in almost every wall. Whether it’s to attach shelves, signs or decorative objects to the wall – almost everyone has already inserted a screw hook into a wall. However, with such conventional hooks, unsightly effects or even damage can occur already during the screwing process but also later during use:
- If the screw hook is to be aligned vertically, the clip often does not close up with the wall and an unsightly gap is created. If you want to screw it in all the way, the hook sits at an angle.
- If the material thickness of a round hook, for example, is too thin, the hook will easily deform when it is screwed in or when a load is suspended from it.
- When mounting with pliers, scratches and other material damage quickly occur on the hook.
Fischer offers the solution with the innovative EasyHook system. It converts screws of different sizes into round, eye or angled hooks. The desired hook adapter and optionally a cover ring are attached to the respective countersunk screw and mounted in the wall with the proven DuoPower or DuoBlade plugs. You can even use a cordless screwdriver without damaging any material.

The EasyHook product advantages are obvious:
- Depending on the screw-in depth, the EasyHook can be mounted at different distances from the wall. The integrated predetermined breaking point allows the hook to be flexibly aligned.
- Installation flush with the wall is always possible, no matter how the EasyHook is aligned.
- The screw always bears part of the load and prevents premature deformation of the plastic hook.
The EasyHook can be used in a variety of building materials. You will achieve the highest load-bearing capacity when installing in solid stone. If you also use a DuoPower plug, you can also screw in plasterboard and perforated building materials without any problems. Pre-drilling in wood is not necessary.
Discover the innovative EasyHook range from Fischer!