LED-Beleuchtung im Büro: Kosten runter, Produktivität rauf

LED lighting in the office: Costs down, productivity up

When the nights start to draw in it is a good time to reconsider lighting in the office. LED panels do not just provide well-lit work places. Employers also benefit from them — several times over!

LED lighting in the office

Many offices and business premises are lit by square mounted lamps in the ceiling.

This type of installation uses almost exclusively fluorescent tubes.

Replacing them with modern, precise LED panels not only saves around 50 percent of energy costs, the panels are also virtually maintenance-free. Due to the optimal colour temperature of the light of 4500 Kelvin (K), which corresponds to natural light, LED panels also ensure a pleasant, fatigue-free working environment.

We offer particularly cost-effective models — take a look at our online shop.

Good lighting conditions are not just for health protection

Sufficient light, shadow-free illumination at the workplace is legally prescribed to protect the health of workers.

By using LED panels, entrepreneurs underline their commitment in the areas of environmental protection and corporate social responsibility.

The light colour of LED panels facilitates comfortable and fatigue-free working and thus directly increases the motivation of employees. Optimal lighting conditions make a significant contribution to the productivity of the business.

Long-life LEDs reduce operating and maintenance costs

Standardised LED panels can be easily and quickly installed in both existing and new panelled ceilings.

Thanks to their class A energy efficiency rating, it is worth exchanging existing lights even just for future power savings.

The maintenance costs, previously incurred through the replacement of faulty bulbs, are significantly reduced thanks to the very long-life LED panels.

LEDs usually last around 20,000 operating hours.

Image source: Fotolia, 77695752, virtua73

Leave a Reply

Your email address will not be published. Required fields are marked *