Modern installations require more than just a functional connection. They demand speed, reliable processes and long-term stability. Spring-loaded terminals consistently meet these requirements. They simplify installation, enhance operational reliability and reduce maintenance costs. This is why they are now considered state of the art in many applications and have become an indispensable part of modern electrical installations.
From screw connections to spring-loaded mechanisms – a technological shift
Since 1951, WAGO has specialised in developing spring-loaded connection technology. The idea is to secure conductors using a precisely defined spring force rather than screws.
Introduced in 1977, the CAGE CLAMP® technology created a universal connection capable of accommodating a wide variety of conductor types without the need for retightening, torque control or time-consuming pretreatment.
Today, this technology is used in many different applications, ranging from building automation and mechanical engineering to demanding industrial environments.
The principle is that of a constant spring force instead of torque
While the correct tightening torque is important for ensuring the quality of the connection in screw terminals, spring terminals use a precisely defined spring force to ensure proper contact.
The conductor is automatically pressed against the busbar with consistent pressure. There is no need for over-tightening, under-tightening or readjustment. The result is a permanently stable and reproducible connection, regardless of the user.
This operating principle forms the basis of WAGO’s CAGE CLAMP® technology and explains its practical success.
Ten reasons why spring clamps are a popular choice today
- It’s simple: just connect with ease
Open the spring and insert the conductor. No need for torque or readjustment. - Fast – save time with every installation
No screws, no tightening required. This significantly reduces installation time, especially for serial wiring or large projects, and boosts productivity. - Secure – defined contact force
The spring automatically adapts to the conductor. It neither damages nor loosens the connection. The connection remains reliably stable. - Consistently high quality, operator-independent
Whether you’re a trainee or a professional, you can expect consistent results. The defined clamping force eliminates uncertainties caused by torque. - Reliable, consistent contact quality
What about temperature fluctuations, stress or power surges? The clamping force remains constant. Contact resistance does not change — the connection remains secure. - Durability – built to last decades
Spring-loaded terminals are reliable even in applications with long service lives. There is no loosening and no loss of contact force. - Durable and corrosion- and temperature-resistant
Can be used in demanding environments from -40 °C to +70 °C. The connection remains stable, even under difficult conditions. - Vibration-resistant – withstands strong vibrations
Machines, vehicles, and industrial equipment place high demands on components. The spring technology withstands vibrations without coming loose. - Maintenance-free: less servicing, more uptime
There is no need for tightening or regular inspections. This saves time and money, and reduces unnecessary downtime. - Versatile: suitable for virtually all types of wire
Spring clamps offer maximum flexibility for single-strand, multi-strand and fine-strand wires, often without the need for pre-treatment.
Spring clamps in action: Faster and easier
Case Study 1: Increased Efficiency in Control Cabinet Manufacturing
A medium-sized mechanical engineering company manufactures complex control cabinets for production facilities. High wiring density, tight deadlines and rotating assembly teams are all part of their everyday operations.
Since switching to terminal blocks with spring-clamp technology, however, wiring time has been significantly reduced. Installers can work faster because they no longer need to account for tightening torque. At the same time, the error rate has decreased because each connection is automatically established with a defined spring force.
This means the company can now plan production times more accurately, reduce rework and improve process reliability right through to delivery.
Case Study 2: Maintaining Flexibility During Ongoing Building Operations
An electrical contractor is responsible for managing the technical infrastructure of a large office complex. Work areas are regularly reconfigured, lighting systems expanded and control systems adjusted.
Thanks to spring-loaded terminals with lever technology, conductors can be quickly and easily disconnected and reconnected without the need for special tools or the risk of incorrect tightening. At the same time, the connection remains permanently stable, even when changes are made frequently.
The result is reduced service requirements, faster adjustments and trouble-free ongoing operation.
The real highlight is process reliability
The greatest advantage of spring-loaded terminal technology does not lie in any single feature, but in the combined effect of all its characteristics.
Spring-loaded terminals facilitate predictable electrical connections: they reduce installation time, minimise sources of error and require no maintenance. While torque used to be the deciding factor for quality and safety in screw connections, the spring now ensures consistently reproducible results.
This means fewer uncertainties during installation, lower maintenance requirements during operation and long-term contact stability, even under load. Last but not least, CAGE CLAMP® technology, developed by WAGO, has played a key role in achieving this level of process reliability in practice.
Greater efficiency. Greater security. Less effort.
Modern installations require more than just a functional connection; they demand speed, reliable processes, and long-term stability.
Spring-loaded terminals consistently meet these requirements, simplifying installation, enhancing operational reliability and reducing maintenance costs.
Consequently, they have become the standard for modern electrical installations in many applications.
Illustrations: WAGO