Spending the holiday on the campsite or experiencing outdoor adventures in a tent is very popular. Camping newcomers as well as experienced campers have to ensure that the camper or caravan has suitable and functional equipment for a successful experience – and the power supply should by no means be neglected. Brennenstuhl has the right tips for power distribution products and offers bright camping accessories.
Which socket for the electricity connection when camping?
As soon as the camper or carvan is stationary, the first step is often to supply the vehicle with electricity. The blue CEE plug, also known as a caravan or camping plug, is plugged into the campsite supply station and connected to the vehicle’s CEE plug. As soon as the 3-pin CEE plug is plugged into the blue CEE socket, it protects the vehicle battery and supplies all electrical devices in the mobile home with electricity.
The voltage range from 200 V to 250 V is marked in blue throughout Europe. The advantage of the blue CEE plug is that it is suitable for permanent use. The CEE 230 V plug promises continuous currents of up to 16 A and very safe use. The cover meets the IP44 degree of protection required for outdoor use, protection against foreign objects and splash water.

Camping power supply requirements — What do campers have to watch out for on the campsite?

The right connection cable What are required are so-called heavy rubber hose lines with the Line designation H07RN-F (or equivalent).

The right cable length The maximum cable length of 25 meters (+/- 2 m) for connecting the caravan must not be exceeded.

The correct conductor cross-section A minimum cross-section of 2.5 mm² is specified for the connection of caravans and mobile homes with a rated current of 16 A. A smaller conductor cross-section is not permitted for connecting caravans or mobile homes on campsites.

Use signal colors The orange signal color draws your attention and those around you to cables lying around and potential tripping hazards.

Matching plugs & couplings For camping and caravan use, plugs and couplings as well as sockets must be at least dust and splash-proof (IP44) when plugged in.
Camping cable reel or camping extension cable?
Often the power supply from the camping distributor to the caravan or camper is not enough. Power is also required for several end devices outdoors, under the awning or in the awning. Not enough slots is often a problem. Cable drums or power stations, which also have CEE and earthing contact sockets, offer a wide range of connection options.However, if the camping cable drum with 25m cable is too long, a camping extension cable may be the better solution. Depending on the distance to the camping junction box, Brennenstuhl recommends taking both products for the camping electricity connection with you: 25m camping cable drum and a camping extension cable. Brennenstuhl also offers power stations and a camping adapter set.
Camping lamps and outdoor lamps as the perfect addition to your outdoor adventure
Camping lamps and hand lamps are standard equipment for outdoor activities such as camping, festivals and staying in tents and caravans. Brennenstuhl offers outdoor lamps with various functions. There are LED lights with music playback, with dimmable light color and integrated power bank or as an inflatable LED outdoor light.Brennenstuhl has the right products for a carefree camping holiday for all camping fans. All products can be found in the reichelt online shop.
Images: Brennenstuhl