Brits want to use voice controlled Smart Home devices, but don’t know how

Brits want to use voice controlled Smart Home devices, but don’t know how

Over half of Brits are or would consider using the likes of Alexa, Siri & co

 

Our research into UK electronics use has revealed that over 56% of Brits are already using or would consider using voice-controlled connected devices in the home, however most of them (55%) don’t know how to install these and would need professional help.

The enthusiasm for state-of-the-art technology in the home is also apparent with systems like Amazon Alexa, Google Home or Microsoft Cortana. While 50% percent of respondents would consider installing a voice-controlled solution, 6% already use the new technology in their home.

In the case of voice-controlled home automation solutions, the desire to operate heating and lighting either automatically or remotely is the first priority (74%), closely followed by home security with camera surveillance/alarm systems (48%) as well as kitchen and household appliances (40%).

Germans are more confident than the Brits to install

Across Europe the trend is similar. Our research found that most German (70%) and French (63%) people surveyed were the same as the Brits, however about half of Germans would do it themselves. 49% – and for men it is as much as 60% – are confident, according to our survey, to be able to accomplish the installation of home automation itself without a specialist. At least 16% believe that they can design and install their own system with electronic components.

Digital natives pay attention to privacy

Of the 30% who wouldn’t consider using devices like Alexa, Siri or Google Home, this was due to concerns over data protection. This is especially striking in the age group of the 18- to 24-year-olds. Digital natives are of the age group most interested in new technology. Those in this group who do not want to use them (40%) clearly state privacy concerns (65%).

Siri and Alexa, but only at home, not on mobile

Alexa, Google Home & co. are generally well received by the majority of respondents for the home. This is very different for mobile. Only 29% of the interviewees use the voice assistant on their smartphone regularly (at least every other day) while 60% indicated they never used it or did not have a mobile phone with a voice assistant.

Photo credit: Fotolia_86290426

Leave a Reply

Your email address will not be published. Required fields are marked *