Cable and wiring testers: quickly identify and rectify network faults

Whether in a corporate network, a building installation or a home network: faulty cable connections can impair data transmission or bring entire network segments to a standstill. Cable and wiring testers help to systematically track down connection problems, check cables and ensure the cabling is functioning correctly. But which test device is suitable for which application?

Why is cable testing essential for reliable networks?

As demands on speed and availability increase, so too does the importance of reliable network infrastructure. Even minor errors during installation can lead to connection drops, reduced transmission rates, or unstable network connections.

Typical causes include damaged cables, incorrectly terminated wires, faulty connectors, and unsuitable cabling. Troubleshooting can be particularly time-consuming in larger networks without the right testing equipment.

This is where cable and wiring testers come into play. They check electrical connections, detect wiring faults and, depending on their specifications, can also help pinpoint the location of faults.

From simple cable testers to professional network testers

Not every test device offers the same range of functions. The choice depends on whether you simply need to check a cable connection, investigate a network fault or verify the performance of an installed cabling system.

Simple cable and wiring testers primarily check for correct pin assignment. They can detect open circuits, short circuits and swapped wires, for example. This makes them particularly suitable for quickly checking newly terminated network cables. A cost-effective option is the UNI-TREND UT681L, which tests RJ45 network cables, telephone lines and ISDN lines. Its LED display allows breaks, short circuits and wiring faults to be identified quickly. This makes the device ideal for simple installation and maintenance tasks.

Advanced network testers offer additional diagnostic functions, such as measuring cable lengths, locating faults, and checking the power supply via Power over Ethernet (PoE). The UNI-TREND UT685B KIT is one such example, using TDR technology to measure cable lengths of up to 500 metres and locate faults. The device also tests RJ11, RJ45 and coaxial cables, and recognises various PoE standards.

Professional qualification and certification testers, such as the WireXpert 500 cable certifier, offer an even greater level of functionality. They analyse the transmission characteristics of the cabling and, with the appropriate equipment, can verify compliance with defined cabling standards.

Identifying typical network faults

Various fault patterns can occur during the installation and maintenance of network cables. Modern testers help to identify the cause of these faults.

Fault patternPossible cause
Open circuitDamaged cable or missing contact
Short circuitUnintended contact between wires
Transposed wiresIncorrect pin assignment
Split PairIncorrectly assigned wire pairs despite a potentially correct pin-to-pin connection
Unstable data transmissionThis can be caused by damaged cables, poor contacts or increased signal interference.

An important function is the wiremap test. This checks the assignment of the individual wires and, depending on the test equipment used, can also detect more complex wiring faults.

Time Domain Reflectometry (TDR) is often used for more precise fault localisation. In this process, the measuring instrument sends electrical pulses through the cable and analyses their reflections. This enables the distance to a break or short circuit to be estimated, for example.

Checking PoE: Data and power over a single cable

Power over Ethernet (PoE) supplies compatible network devices with electrical power directly via the Ethernet cable. This technology is used in devices such as IP cameras, Wi-Fi access points, and VoIP telephones.

In the event of faults, it is therefore necessary to check the data connection and, where applicable, the power supply.

Specialised PoE testers can display information such as the applied voltage, the PoE standard in use and the wire pairs being utilised. Some models can also measure current consumption and power under load.

One such model is the Delock 63110. This device checks the pin configuration of RJ45 network cables, detecting open circuits, short circuits and swapped wires. It also supports testing PoE power sources in accordance with IEEE 802.3af and 802.3at standards. When a load is connected, the tester can display the voltage, current and power.

Fibre-optic networks: measuring optical power and attenuation

Alongside traditional copper cables, fibre-optic connections are becoming increasingly important in corporate networks, data centres, and building infrastructure.

Unlike copper cables, data transmission here takes place via light signals. The test procedures therefore differ accordingly. Our guide, Basics of Fibre Optic Technology – Understanding and Using Fibre Optics at Home, explains how fibre-optic technology works, the different types of cable available, and the important factors to consider during installation.

One of the most important parameters is optical attenuation. This describes the loss of light power along a fibre-optic link. Excessively high attenuation values can be caused by dirty connectors, unfavourable bend radii, or damaged fibres, for example.

Such tests are performed using optical power meters and light sources. These devices enable the measurement of light power and the determination of link attenuation.

The FiberMASTER from TREND Networks combines an optical power meter with a light source. This makes the device suitable for testing and troubleshooting fibre-optic connections.

OTDR testers are also available for more in-depth analysis. These use reflected light signals to locate events along a fibre-optic link, enabling examination of splice points or damage, for example.

Which cable tester is suitable for which application?

The appropriate test instrument depends primarily on the application and the level of detail required for the measurement.

Area of applicationUseful test functions
Home network and simple installationWire assignment, continuity, short circuit
In-building network cablingWiremap, cable length, fault location
IP cameras and Wi-Fi access pointsRJ45 testing, PoE voltage and, where applicable, power
Professional network installationQualification or standards-compliant certification
Fibre-optic installation and maintenanceOptical power, attenuation, OTDR where necessary

It is important to distinguish between a basic functional test and a thorough analysis of transmission characteristics. For example, a cable may be electrically connected correctly yet still fail to meet the speed requirements of a specific network.

Reliable networks start with the right testing

Cable and wiring testers simplify fault-finding and help identify network problems at an early stage, whether for new installations, expansions or maintenance. While compact devices suffice for basic wiring tests, professional measurement systems offer comprehensive diagnostic and documentation capabilities.

Reichelt Elektronik offers a wide selection of Cable and wiring testers to suit a variety of requirements. The Tools for Cat Technology category also provides suitable accessories for installing and maintaining network cabling.

Images: Adobe Stock