Protettore di sovratensione RJ45 Protezione contro le sovratensioni, ad es. da fulmini! €16,95 €24,95
IP Homematic - Pacchetto di sicurezza Access Point, Sirena interna, Rilevatore di movimento, Sirena esterna €199,00 €239,80
Softpress cucitrice piatta riduce la forza richiesta fino al 60% rispetto alle cucitrici convenzionali Leitz. €18,90
Maglia veloce WLAN nella rete domestica del FRITZ! Il ripetitore FRITZ! 1200 aumenta la portata di qualsiasi WLAN in modo semplice e veloce €63,90
Epson WorkForce WF-3720DWF Dispositivo multifunzione 4 in 1 con stampa Wi-Fi, Wi-Fi Direct e duplex €89,90 €119,90
Scanner portatile per libri Scansione sempre e ovunque con IRIScan™ Book 5. Con batteria agli ioni di litio. €89,00 €129,00
Candela Osram SMART+, E14, A+ [A ++ - E] corrisponde a una lampada a incandescenza da 40 W. €11,95 €23,95
Remote controlled digital picture frame with the Raspberry Pi Digital picture frames are among the most popular Raspberry Pi projects. In this How-To we show you...
Production of supercaps: Korchip replaces Panasonic The South Korean company Korchip was founded in 1990 and has since developed into a specialist for ...
DJI Osmo Mobile 3 Gimbal: High-quality videos through intelligent gesture control If you want to produce high-quality videos with your smartphone, you can use a gimbal to significan...
Application examples for highly sensitive leakage current clamps Leakage current clamps are valuable diagnostic instruments for the electrical and electronics profe...
New in the range: Inductors from FASTRON FASTRON was founded in 1978 in Munich and is a well-known brand name for inductors. FASTRON operate...
DELOCK WLAN socket outlet switch adapter with TASMOTA firmware Cloudbased socket switches for 20€ are now available in stores, but the new 11826 adapter from...
Z-Wave Technology: Smart Home for Makers There are now many ways to make your home smart. However, most solutions are severely limited by th...
The DisplayPort™ Interface – What is DisplayPort™? DisplayPort™ is a universal connection standard standardized by the VESA (Video Electronics S...
Converting Benchtop Oscilloscopes for Field Use For many users, whether private or commercial, an oscilloscope is a high-priced but universal measu...
Ultimaker Cura 4.2 beta: What’s new? Just recently the new beta of Ultimaker Cura 4.2 was released. Below we present some new features t...