Topic-Explorer – building and energy management

Topic-Explorer – building and energy management

As much as necessary, as little as possible! Most energy is still derived from fossil energy sources and is used to heat a building or for lighting, computers, ventilation systems, refrigeration and cooling equipment, pump systems and motors, etc… In addition to the problem that these energy sources produce carbon dioxide when burned and thus increase the greenhouse effect, they are not infinite. Energy prices are currently exploding and, as a result, the costs for both private consumers and companies.

Energy management includes the planning and operation of generation and consumption units. Discover energy management products and systems in our extensive range to conserve resources, protect the climate, reduce costs and ensure energy requirements.


Explore further articles:

  • LED drivers – the key to an efficient lighting solution

    LED drivers – the key to an efficient lighting solution

    LED bulbs are practical and popular because they are energy-efficient, long-lasting and low in heat generation. But to work properly, they need a different voltage than usually comes from the socket. That’s why people often talk about LED drivers, which are used for bridging. However, the term regularly causes confusion. This guide shows the differences


    Read now ►

  • With LOGO! 8.3, the popular Siemens small controller is connected to the cloud

    With LOGO! 8.3, the popular Siemens small controller is connected to the cloud

    With cloud connection for more efficiency and flexibility The new version 8.3 has a cloud connection, bringing the possibilities of a smart factory to even the most compact automation project. For example, measured values for key indicators of the condition of a machine or plant can be collected and evaluated to prevent errors as well


    Read now ►

  • LED for any purpose – optimal and energy-efficient light installations for workspaces

    LED for any purpose – optimal and energy-efficient light installations for workspaces

    A guide to the possibilities, plus tips when buying It is fundamental your working environment is lit correctly for safe, easy working, whether in workshops or industrial areas, as well as in the office, as the eye takes most of the strain during office work. Productivity is directly influenced by light, as poor lighting is


    Read now ►

Leave a Reply

Your email address will not be published. Required fields are marked *