PC aufrüsten – Das müssen Sie beachten, damit ihr PC wieder schnell wird

How to upgrade your old PC

Working with an older PC can be frustrating because of the slow load times and ancient software but it doesn’t have to be this way. In this guide, we share tips on how to upgrade your PC and which components matter most. First let’s run through the basics, what kind of performance is actually required?

Typical applications

Office

For office applications like word processing, e-mail and the internet, a low-cost processor (e.g. from AMD or Intel) and at least 4 GB of RAM is sufficient. If you also want to edit your holiday photos or like to surf with many browser tabs, choose 8 GB. An extra graphics card is usually not necessary. When choosing a processor, care should therefore be taken to ensure that this includes an integrated graphics solution. A noiseless SSD hard drive is a useful upgrade and ensures fast program starts and short boot times – thus saving your time and nerves.

Multimedia

For video editing, it‘s crucial to have sufficient RAM available. At a resolution of 1080p, it should be at least 8 GB, at 4K at least 16 GB and at 8K you should already keep 32 GB as a precaution. Since both photo and video editing are very write- and read- intensive, it’s worth investing in an SSD. A graphics card that supports OpenCL or CUDA is also worthwhile as professional software like Adobe Premiere uses it for calculations.

Software development

Modern development environments benefit from generous memory, 16 GB or more is recommended. In addition, projects often consist of many small files that are analysed by the appropriate tools – an SSD speeds this up considerably. Memory and SSD are therefore more important than the fastest CPU. A simple on-board graphics card is often sufficient for the graphics. If you work with more than one screen, you should make sure that the appropriate connections are available.

Gaming

For gaming PCs, the following applies to all components: more is better. A fast processor and a good 3D graphics card are a must for a smooth gaming experience. 16 GB RAM is now the minimum requirement for most modern games. An SSD is not absolutely necessary but ensures faster program starts and significantly shorter loading times. Especially in multiplayer games, an SSD is therefore not only a pleasure for a self but also for all other players.

The most important components and how they interact

MotherboardSchwarzgraues Mainboard für den PC

Everything comes together in the motherboard. It‘s important that the desired processor and memory are supported. The expansion slots are usually only needed for graphics cards. Network and sound are already integrated on most motherboards. If you use a lot of external devices, you should pay attention to the number of USB ports.

Furthermore, it is to be seen which PCIe generation is supported, so that correspondingly fast M.2 SSDs can also exploit their full potential. If you do not want to use your own graphics card, make sure that the motherboard has the right connectors for your monitor or organize an adapter. The motherboard also specifies how many USB ports of which type your system has. You can only gain more through a hub or a PCIe USB card.

If you want to install many hard disks or SSDs, you should also pay attention to how many SATA connectors your motherboard supports. For SSDs, as already mentioned, the M.2 number is also important.

The form factor indicates the size of the motherboard. Most PCs have motherboards in ATX or µATX format. The latter is smaller and therefore usually has fewer slots for extensions such as graphics cards.

If you want to make your computer unique or overclock your system, you should pay attention to how many fan connections the motherboard has and whether it has RGB headers for illuminated fans / RGB stiffs.

Main Memory (RAM)

RAM Arbeitsspeicher in schwarz und orange für den PC

The rule of thumb is: the bigger the amount of data you work with, the bigger the memory should be. If the memory available is not sufficient, the slower hard disk will be used.

The maximum amount of memory you can have depends on the operating system, the motherboard and the processor. If the operating system is the 32-bit version, a maximum of 4 GB is possible. A 64-bit system supports a maximum of 128 GB. With Windows you can find this information in the system properties. Find these by pressing the ‘Windows’ and ‘Pause’ keys at the same time. How much memory the mainboard and the processor support can be found in the manufacturer’s specifications. If motherboard, processor or operating system have different memory capacities, then the smallest specification is considered a limit for your system.

When selecting memory modules, three things are important:

  • Design: PCs usually use DIMM modules, laptops and Mini-PCs frequently use the smaller SO-DIMM.
  • DDR generation: Modern PCs work with so-called “Double Data Rate” modules, or “DDR” for short. These can be divided into different, incompatible generations. The interruption in the contact strip prevents you from accidently installing the wrong generation model.
  • Clock frequency: The clock frequency of the RAM can be selected theoretically, but all modules use the speed of the slowest module.

Tip: If you want to upgrade the existing RAM, it is best to use the existing modules.

Storage

Eine offene interne Festplatte für den PC

Hard drives are divided into classic HDD hard disks with magnetic disks and SSD hard disks, which function similarly to memory cards or USB sticks.

While classic hard drives are much cheaper, especially for large amounts of data, SSD hard disks are fast because they have moving parts. Classic defragmentation is a thing of the past. The advantages are easy to see when working with multiple files, starting the PC or individual programs. SSD hard disks are also completely silent, which it a nice side effect!

When making your selection, pay attention to the design (e.g. 2.5″, 3.5″ or M.2 for some Mini-PCs), which depend mainly on the PC case. On the other hand, the type of connection is important – usually SATA.

By default, a system should have both an SSD, for the operating system and frequent or demanding programs, as well as an HDD, for files and resource-saving programs, in order to combine the advantages from both areas.

Processor (CPU)

For processors, it is important to pay attention to which processors the motherboard supports. The decisive factor is whether you have an AMD or an Intel board and which socket is installed.

Pozesso für den PC von Intel in blau und pink

The most important characteristics of a processor are:

  • Clock frequency: The clock frequency indicates how fast the processor can manage instructions. Processors with a higher clock frequency are faster than comparable processors with a lower clock frequency, but use more energy.
  • Number of cores: Each core can serve a process simultaneously. Most processors support at least two, which is sufficient for simple applications. For more demanding applications, we recommend four cores.
  • Cache: The fastest cache in the PC . Data that does not fit into the cache is retrieved from memory.

Processors usually specify type and clock frequency for the supported RAM modules. These should be matched, since faster RAM modules are technically possible, but don‘t carry any advantages. There is also an upper limit for the maximum amount of RAM the processor can support.

Please note: The most powerful processors can only be used sensibly if the other components are fast as well. The CPU and motherboard must be compatible. The mainboard manufacturers offer lists of supported CPUs for each mainboard.

Graphics card

The graphics function in the processor is usually sufficient for simple applications. For more demanding applications (e.g. photo and video editing or gaming) or when working with multiple monitors, a dedicated graphics card makes sense. With powerful graphics cards, you should make sure that the PC power supply is sufficiently strong.

The most important features of a graphics card are:

  • GPU clock: This value indicates the speed of the graphics processor (GPU).Grafikkarte mit zwei Lüftern in schwarz
  • Graphics memory and bandwidth: In order to exploit the high performance of the GPU, the current required data is transferred from the main memory to the memory of the graphics card. The graphics memory is permanently installed and cannot be expanded. The bandwidth indicates how fast data is transferred to the graphics memory.
  • Shader units: The number of shader units is a measure of how many of these calculations the GPU can perform simultaneously. What was originally developed for 3D graphics is now also used by other applications such as video editing software.

Tip: Graphics cards differ in dimensions. Some are slightly longer than others, and some need the space of two expansion cards because the fan is so large. So make sure the graphics card fits into your PC.

Upgrade your PC with an easy upgrade set

Upgarde sets are a simple and cost-effective solution for updating your PC. These include components that have been tested together and are compatible. As a rule, a tuning kit contains:

  • A motherboard
  • A processor with cooler
  • And the main memory

You don’t just save on planning, you also get the whole PC up to scratch in one go. And because you buy the components as a set, they‘re even cheaper. All upgrade modules have illustrated installation instructions so upgrading is a breeze.

Build your own PC with an upgrade set

Upgrade modules are also an easy way to build the PC you want. A suitable empty ATX housing with power supply unit, the desired upgrade module and the appropriate hard disk, and the individual PC is all you need to get going.

Cover picture: Adobe Stock

Leave a Reply

Your email address will not be published. Required fields are marked *