Tragbare Monitore von Verbatim

Verbatim’s portable monitors

Mobile working has long been ubiquitous – usually on a laptop or tablet, but also on a smartphone if necessary. In doing so, the user often feels restricted in one way or another – the working process only flows haltingly or a certain discomfort creeps in. For more efficiency and comfort, a second screen is often needed. The new portable monitors from Verbatim provide the solution. They are now available in the online shop.

Verbatim portable monitors

Ultimate flexibility

Verbatim’s portable monitors offer a wide range of everyday uses: on the go, at home, in public, for gaming or to increase productivity. The compact models can be used individually or as an additional screen for the laptop, as a large display for the smartphone and tablet or even as a portable console.

Portable screens in Full HD

There are two models in three different sizes (14; 15.6; 17.3 inch) available in the reichelt online shop. The Verbatim displays in 16:9 side ratio have IPS panels with a particularly wide viewing angle of 178° and shine with a Full HD resolution of 1920 x 1080 and 16.7 million colours. HDR technology provides a first-class picture experience.

Maximum compatibility over one cable

The lightweight monitors are connected to the main device – PC, Mac, tablet, smartphone or console – using USB-C or HDMI. Power, data and image signal can be transmitted by a single cable. If HDMI is used, an additional power supply unit (included in the scope of delivery) should be connected in between. The advantage here lies in the additional use of the USB-C port.

Spoiled for choice with USB-C or HDMI

Equipment with and without touch screen

Verbatim also offers one of its two new models in a touch screen version. The display reacts quickly to finger or pen touches and can be operated intuitively with 10-point touch functionality. Gestures, swipe, scroll, drag and pinch make it easy to use. The touch models are also equipped with a robust aluminum housing.

VERBATIM 49590VERBATIM 49591VERBATIM 49592VERBATIM 49593
no touch screenwith touch screenwith touch screenwith touch screen
14 inch14 inch15.6 inch17.3 inch
760 g860 g980 g1,540 g

Images: Verbatim

Leave a Reply

Your email address will not be published. Required fields are marked *