Sicherheit mit Stil: Die neuen Farben der Ledger Krypto-Wallets

Safe and stylish – the new colours of Ledger crypto wallets

The Paris-based company Ledger is an A-brand among wallet manufacturers and deals with encryption technology. The Ledger models perform very well in comparison tests in the categories of functionality, security and price-performance ratio. The wallets are particularly suitable for beginners in the world of cryptocurrencies. Regardless of whether it’s old-fashioned on paper or ultra-modern via an app – there are many ways and means to store private keys securely. Each of these methods comes with its own advantages. Hardware wallets form the bridge between the two approaches by combining the advantages of both methods. The private keys are stored offline on a USB stick, which is only connected to a computer whenever you want to access purchased cryptocurrencies, such as Bitcoin or Ethereum and, for example, NFT. Safe storage of private keys can be very easy and also so colorful. The successful and reliable crypto wallets from Ledger are now available in three new colors in the reichelt shop.

Three new colors for the Ledger Nano S Plus and Ledger Nano X

Drei neue Farben für den Ledger Nano S Plus und Ledger Nano X
The new colors: Amethyst Purple, Pastel Green and Retro Gaming
Not only do you keep your crypto assets safe and reliable with Ledger’s crypto wallets, but they now also look really good. The Ledger Nano S Plus and the Ledger Nano X are now available in the colors Pastel Green, Amethyst Purple and Retro Gaming. It doesn’t just have to have aesthetic value. The different colors can be used wonderfully for self-organization if you use more than just one ledger. For example, each color can have a different purpose.

Aesthetics meets functionality

Der Ledger Nano S Plus schützt Ihre Krypto-Werte mit einem CC EAL5+ zertifizierten Sicherheitschip.

In addition, Ledger’s crypto wallets are quite impressive in terms of functionality. The Ledger Nano S Plus protects your crypto assets with a CC EAL5+ certified security chip. The large display also makes navigating and verifying transactions a breeze.

The Ledger Nano X even goes one step further in terms of functionality. With its Bluetooth feature, you can access your cryptos and NFTs anytime, anywhere. The 100 mAh battery makes it possible. In contrast to the Ledger Nano S Plus, the Ledger Nano X does not have to be connected via a cable. It works for several hours at a time even without charging. Thanks to its iOS compatibility, you don’t have to accept any restrictions.

Images: Ledger

Leave a Reply

Your email address will not be published. Required fields are marked *