The Joy-IT DMSO2D72 is a real all-rounder, because it contains three functions in one handy device: A 2-channel oscilloscope, a signal generator that records any type of wave, and a multimeter that has six different measurement types. The multi-function measuring device is in no way inferior to comparable individual devices in terms of its range of functions.
This has the immense advantage that only one instrument needs to be installed at the workplace instead of three space-consuming instruments. For mobile use, there is no need to transport various devices that may be difficult to transport – the combination of three devices in one therefore offers great advantages for both stationary and mobile use.
The price is very attractive for the wide range of the device and the available usage functions.
Easy handling for special user comfort
Working with the measuring device for any requirement is additionally facilitated by the fact that it can be operated very easily and clearly via a “one-button” auto measuring function and “one-button” page out. The 2.8 inch 65K colour LCD display also allows two signals to be directly compared.The 18650 lithium batteries last up to one day on standby for several weeks when used constantly. They are charged in a timely manner via a USB-C interface, which is also possible while the device is in use. In addition, the device is coated with silicone, which protects it from various environmental influences in outdoor use.