antennas from Poynting

Perfect wireless networking – thanks to the multi-frequency antennas from Poynting

The new mobile communications standard 5G is in the starting blocks and will gradually be rolled out across Germany. Companies in particular see great opportunities in the new mobile communications standard to be able to implement advanced technology. As a study by reichelt from 2020 showed, 36 percent were planning to invest in 5G in 2021. With antennas from Poynting, you can make your company fit for the new technology. The diverse product portfolio is now available in the reichelt online shop and is a more than sensible addition for routers of the TELTONIKA brand for example.

From South Africa to the world

From its headquarters in Samrand, the business centre of Johannesburg, Poynting supplies and supports business customers worldwide with more than 70 distributors – and has been doing so for more than 30 years. The increased demand has even led to the opening of new regional branches in Munich and Mansfield, Texas. In this way, the company, whose name is derived from the Poynting vector – an electromagnetic directional measure – can ensure that it can also offer its customers the best solution locally.

With decades of experience, Poynting provides the optimal solution for every individual requirement profile in a wide range of industrial areas – from LTE, 5G or Wifi to RF and other applications. In addition, the company now holds more than 50 patents and designs for unique antenna solutions for improved communication at broadband level.

Defying wind and weather – the POY OMNI-280-01

Whether wall-, pole- or magnet-mounted, the POY OMNI-280-01 can be fixed in the desired place in no time at all. The weatherproof housing ensures that the broadband antenna can withstand temperatures ranging from -40°C to 70°C. It can be installed virtually anywhere. This means it can be installed virtually anywhere.

The omni-directional approach allows you to upgrade the current 4G standard to 5G as soon as it becomes available. In addition, the antenna is backwards compatible with all previous mobile standards, stabilising your connectivity for the long term and improving the user experience. The antenna is perfectly designed to increase the signal strength of industrial routers. This allows you to achieve higher data throughput with a stable as well as high-quality connection on the ultra-wideband spectrum.

2-in-1 solution for automotive and transport

With a covered ultra-wideband spectrum from 450 MHz to 3.5 GHz, the POY MIMO-3-12 is perfectly suited for mobile applications. This performance enables the combination with routers from different operators. The weatherproof as well as waterproof design according to IP 68 allows main applications such as transport and shipping at temperatures from -40°C to 80°C. The combination of two mobile MIMO antennas and perfectly balanced radiation patterns guarantees the stable use of different radio technologies. Thus, it is not only 5G-ready, but can also be easily extended to a bandwidth of 3.8GHz, allowing the antenna to perform even more 5G applications.

Whether at the industrial site or for your vehicle fleet: If you want to make your company future-proof or update your industrial routers, Poynting also offers the perfect solution for your individual requirements with its broad product portfolio. The various powerful broadband antennas from the South African manufacturer are now available in the reichelt online shop.

Image: Adobe Stock/Poynting

Leave a Reply

Your email address will not be published. Required fields are marked *