Walsin Technology’s product range includes various types of resistors such as chip resistors, metal film resistors, thick film resistors and wire wound resistors. The company also produces a wide range of capacitors such as ceramic, tantalum and aluminum electrolytic capacitors, as well as coils, chokes and filters in the inductor category. These products are used in various industries such as telecommunications, automotive, medical, aerospace and home appliances.
Walsin Technology also strives to produce environmentally friendly products and is committed to promoting sustainable developments. The company has a strong R&D department focused on developing next-generation products. Through continuous investments in research and development, Walsin Technology relies on innovative technologies and an expansion of the product range.We have recently added Walsin products to our range and have initially included more than 400 products from the extensive range of manufacturers in our portfolio. These include the SMD ceramic capacitors in sizes 0402, 0603, 0805 and 1206 of the X7R specification and the SMD resistors in sizes 0402, 0603, 0805 and 1206 in 1% of the E12 series.
As usual, all products can be purchased from 1 piece, from 100 pieces or in roll size (up to 10,000 pieces) at attractive prices.
Images: Adobe Stock