With the SONOFF WLAN system, the home electrical system of every home becomes smart. The electrical switches and adapters communicate via WLAN and can conveniently control connected devices or sockets via eWeLink App (Android and iOS) via a mobile phone, home automation server or browser.
The WLAN switches from SONOFF transmit data via the WLAN router to a cloud platform via which the user can remotely control all devices integrated into the Smart Home system. All this is done via Amazon’s globally available AWS server.
The SONOFF WLAN adapters can be easily integrated into existing electrical installations – whether in a new building, an existing building or a rented apartment.
What makes the SONOFF WLAN-SYSTEM so special is that it can be individualized.
The inexpensive SONOFF adapters have meanwhile gained cult status. They are a good alternative to other, often expensive, existing systems. The special thing about them is their technical customizability. The app enables the user to create different scenarios. Switching times can be parameterised without much effort. Another positive feature is the adapter’s ability to migrate to the cross-platform ioBroker system. All that is required is a small adjustment.
Personalized Home Automation
No matter in which area of the Smart Home Setup – a WLAN adapter from SONOFF adapts to the individual needs of the user. Using a switching actuator, the lighting can be controlled, the coffee machine preheated in the morning or a smart socket can be programmed.