Those who want to equip their homes with smart technology today are increasingly turning to smart surveillance cameras. With their sophisticated technology, they offer users protection for their own homes. reichelt elektronik offers WiFi-enabled cameras for indoor and outdoor use as well as the smart video doorbell from Laxihub.
Wireless technology from the Netherlands – for the whole world
Laxihub is a new brand from Arenti Technology. The company offers its worldwide customers reliable security solutions – regardless of whether at home or at work. The Dutch company, with its headquarters in Hoofddorp, relies on wireless surveillance cameras with easy installation that can be integrated into the local WLAN in no time using the Arenti app.
The perfect choice for indoors and outdoors – Laxihubs surveillance cameras
All cameras save both image and sound in mp4 format on the SD card. In addition, Arenti makes the company’s own cloud available to all users, to which you can easily upload your data.With a resolution of 1080p and sophisticated night vision technology, you can follow what is happening on your property with a razor-sharp image in real time. With the indoor cameras, such as the ARENTI M4-IN1, you also always have an eye on your child or your pets in the next room. Thanks to the built-in microphone, you can also use the Arenti app to communicate via the camera.
Set your outdoor cameras to move with Artificial Intelligence (AI)
In addition to the wide range of indoor cameras, Laxihub also has a large number of outdoor cameras, such as the ARENTI W1, as well as the smart video doorbell ARENTI B1 in its product portfolio. All surveillance cameras for outdoor use are weatherproof according to IP 65 and, thanks to an infrared sensor, are ideally suited to deliver full HD-capable images even at night. Equipped with a 145 ° wide-angle lens, the smart cameras also make it possible to set a large observation radius. Thanks to the integrated AI feature, you can also teach your surveillance camera to react only to actual movements – and not to a leaf blown by the wind or a spider in front of the lens.So if you want to use video and sound monitoring of your own property in the future, you are sure to find the right device with the large selection from Laxihub.
Image: Arenti/Laxihub