Makeblock’s mTiny is the new educational robot from Makeblock for children between four and eight years of age
With the MAKEBLOCK mTiny Discover Kit, Makeblock landed a real hit for digital learning with children last year. The little panda robot is specifically aimed at teachers and children between the ages of four and eight.
Learn to program in a playful way
Nowadays the learning process for children is no longer just analog. Rather, digital devices already help preschoolers to train key skills such as logical thinking. It is less about “just parking the children in front of the screen” and more about making better use of the possibilities of the digital age. With the MAKEBLOCK mTiny Discover Kit, Makeblock has brought the perfect answer to these requirements on the market. The educational robot for children who are growing up in the digital age promotes logical thinking in a playful way and is particularly child-friendly. The panda-look device has no screen and is operated with the accompanying pen. It also includes an intelligent floor mat and various control cards. The preschool children can now use the stick to tap on the mat or cards and thus activate the individual commands on the cards. You can also use mTiny Discover to paint letters and numbers. Teachers can also integrate math and literature concepts.Ideal for schools and educational institutions
The main goal of the mTiny is to teach the children the core components of computational thinking. By using masks and flags, mTiny can also transform itself into different characters, which means that the learning children can also gain socio-emotional learning experiences. In addition, mTiny also promotes fine motor skills and spatial imagination. For teachers, the mTiny provides practical support in everyday school life. Through various activities and lessons, you can train specific areas with the mTiny and use the possibilities of digitization for learning purposes.
Child-friendly design
mTiny is made from environmentally friendly and non-toxic materials. Rounded corners and adjustable brightness and volume also ensure safe learning for the children.