Hydraulic balancing ensures that all radiators and underfloor heating circuits are supplied with heat evenly. In technical terms, this means that each room receives exactly the amount of water it needs, providing the appropriate heating output. This prevents common issues, such as rooms near the boiler overheating or radiators at the end of the heating circuit barely getting warm.
The result is a more stable heat distribution throughout the building. At the same time, the heating system can work more efficiently because less energy is wasted on unnecessary oversupply. This makes hydraulic balancing one of the most important measures for optimising a heating system.

Automate with Homematic IP instead of manual adjustment
In classic systems, hydraulic balancing often requires calculations and manual adjustment of the valves. Homematic IP takes a different approach here. Intelligent components regulate heat distribution during operation, automatically adjusting it to actual demand.The Homematic IP radiator thermostat ‘Evo’, controls the temperature directly at the radiator, thus supporting demand-oriented heat emission. This means that the system controls the heating output not only according to fixed schedules, but also according to the actual room situation.
Incidentally, all other Homematic IP radiator thermostats, in addition to the Evo radiator thermostat, can automate hydraulic balancing.

Precise control for underfloor heating
An even supply is also crucial for surface heating systems. Homematic IP offers motorised underfloor heating controllers for this purpose. These controllers can manage multiple heating circuits within a system, ensuring precise and reliable heat distribution across all rooms.
This is an important step in achieving a balance between comfort and efficiency, particularly in larger living spaces or those with multiple heating circuits.

Modern heating optimisation with a system
Additional variants are also available, including the ‘pure’ radiator thermostat and starter packs for multiple radiators and smart underfloor heating systems. This allows you to create a flexible system, ranging from single rooms to complete heating control.If you want to operate your heating system more efficiently in the long term, hydraulic balancing provides a sensible technical foundation. With Homematic IP, this optimisation can be conveniently implemented and expanded step by step.
Images: Homematic IP, Adobe Stock