Do you know the feeling when the fine hairs on your forearm stand up and a slight shiver runs down your spine when, for example, a band plays its first chords. How nice it would be to be able to experience such a moment more often or not? No more problem with Clicktronic’s premium cables, because with them this experience is just a click away.
Pure copper conductors, gold-plated contacts and multiple shielding help you block out the background noise of everyday life and immerse yourself in an impressive world of sound and images. Find yourself on the festival grounds without having left your sofa at home. Experience thunderous fan chants, just like in the stadium and nuanced film moments, as if you were right in the middle of it.
No signal loss on long meters
For more than 10 years, the German brand Clicktronic has been associated with top-class acoustic and visual enjoyment. With the brand relaunch, adjustments were made where there was still room for improvement: conductor diameters were optimized and technical standards were raised. Bestsellers such as the DisplayPort cable are now available in lengths of 15 and 20 meters. High-speed data transmission is thus also possible over long distances without loss – a plus point that Clicktronic customers have always appreciated.
The solution for connection defects on the TV
Who does not know it – the new flat screen TV has only 2 HMDITM connections but external playback devices such as Blu-ray players, game consoles, Fire TV sticks or receivers want to be connected. This is where the Clicktronic HDMITM Flex adapter comes into play. Thanks to its bendable PVC jacket, it can easily be installed in tight places, such as close to the wall. It serves as a permanently installed interface to which devices can be connected as needed.
Quality you can touch – made in Braunschweig
With around 20,000 entries, the Red Dot Award is one of the largest design competitions in the world. Clicktronic was able to impress the international jury of experts with its innovative packaging concept. The design made in Braunschweig impresses with a color guidance system of strong signal colors. The concise typography, the arrangement of product features and application images contribute to orientation. The wavy spot coatings on the handle edges provide a premium haptic feeling.
Packaging so well thought out that it is almost too good to throw away. Because Clicktronic attaches great importance to sustainability and completely dispenses with plastic with the environmentally friendly cardboard packaging.
10-year manufacturer’s warranty: A connection for decades
From unboxing to years of use of the products – Clicktronic convinces with a continuously high quality. We are so convinced of this that we completely cover you in the first decade with the manufacturer’s warranty.
Have you already clicked through our range? Then explore it here in our reichelt store.
Bild: Clicktronic