Whether in private households or public institutions – surveillance cameras are enjoying growing popularity. But even the best security camera is useless if the battery is empty. And that can happen quickly.
With the surveillance camera from Eufy, users don’t have to worry about maintenance for up to a year – because with one charge, the battery lasts up to 365 days. In the event of a power failure, the HomeBase can maintain monitoring for up to 48 hours with an integrated battery. So you are always protected from intruders.
Robust and uncomplicated surveillance camera
In addition to the long battery life, the camera convinces with its uncomplicated installation. The magnetic holder is simply screwed to the wall – then the camera can be attached and adjusted.
Since the device is completely wireless, users are very flexible when positioning the surveillance camera and do not have to worry about the wiring of contacts. The Eufy camera can be used both indoors and outdoors because it is weatherproof (IP67 class).
Safe in and around the house
Since the surveillance camera records in 1080p HD resolution and has night vision, users are protected from unwanted visitors around the clock.
When the surveillance camera detects an unknown person using person and face recognition, the user receives real-time notification on their smartphone.
For example, the 2-way audio system enables the user to communicate with the unknown person. In addition, an anti-theft alarm signal sounds if there are intruders on the property.
Secure data storage and app access
The recorded surveillance videos are stored locally on an SD card in AES 256-bit encryption. This ensures that the data is secure and there are no additional costs for a subscription to the manufacturer.
The recordings can be viewed at any time in the free app. Even real-time streaming across multiple Eufy surveillance cameras is possible when the user is on the move and wants to make sure that everything is fine in the monitored area.