Keeping an overview of barcode scanners and accessories for cash register or restaurant use or barcode products in industrial environments is no longer an easy task these days. The selection of barcode scanners in all colors, shapes and connections alone increases very quickly into the thousands. A lot of time and energy is lost to find the one solution that meets the respective requirements, fits into the budget and is compatible with all other components.
The ARTDEV product range was developed in such a way as to have an easily understandable but comprehensive range of offers that does not consume a lot of training time or money and attaches importance to the important things. The following three products are available for use in retail, gastronomy and even in the industrial environment of transport and logistics.
Handy, versatile, wired – AS-1320 barcode scanner
In order to simplify the mentioned, complicated product selection, the AS-1320 is available in exactly one configuration: USB and full equipment! There is also no question of the supported barcodes: The AS-1320 supports all common ones – both in the 1D barcode area and in the 2D barcode area. In addition, it always has a stand included in the scope of delivery and, of course, also supports the automatic barcode capture without having to press the trigger on the device. If a customer shows their smartphone with a coupon code – don’t worry: the AS-1320 naturally also reads barcodes from smartphones.Comprehensive barcode solution – Second version of the AS-7210 barcode scanner
This is really suitable for almost every application in which a barcode is to be recorded in whatever form. The first thing you notice is the really handy, small design – smaller than standard smartphones. However, ongoing operation is its real strength: three different operating modes can be selected directly on the device, through which the AS-7210 can be used as a commercially available, wired barcode scanner after connecting a USB connection cable. A second mode activates a Bluetooth mode on the scanner and turns it into a wireless barcode scanner. In the third mode, the focus is on collecting the scanned barcodes on the internal memory. After completing a barcode collection, such as an inventory, it can simply be copied to the PC as a text file with any conventional USB stick.First security feature – AC series cash drawer
Cash drawers should first and foremost offer secure storage of cash. According to this principle, all ARTDEV cash drawers and cash boxes have a robust metal body and are all single or double lockable. For increased security or at the end of the day, cash inserts can be removed, some of them can be closed with metal lids and stowed in the safe. The ARTDEV AC cash drawer series includes cash drawers with widths from 30cm to 42cm (11.81″ to 16.54″), space for up to six different banknote sizes and of course all euro coins and slots for checks and receipts. The opening is usually done electronically by the cash register via the receipt printer. And for applications in which there are no receipt printers, there are also cash drawers that can be opened with a simple push on the front and then pushed back into the lock on the front – completely without an electronic connection and of course still lockable.Image: ARTDEV