Kraftform Kompakt VDE – the ergonomic all-rounder for electricians
If the electrician needs a screwdriving tool that is suitable for as many applications as possible, the Kraftform Compact VDE interchangeable blade system is the right choice. Compact and protected in light and robust textile bags, the Kraftform Compact VDE is also the ideal companion for mobile applications.The sets are individually tested according to DIN EN 60900 at 10,000 volts. The ten times higher test load guarantees safe working at the maximum permitted voltage of 1,000 volts. Blades can be exchanged quickly and easily. If the interchangeable blade is pushed into the holder on the handle, it locks automatically and sits securely and securely. To release it, simply push the shifting ring downwards and remove the blade.
The multi-component ergonomic handle allows a high degree of power transmission, which is achieved thanks to the large Kontaktflächen at hand in the soft grip zone. The hard grip areas, on the other hand, guarantee an almost smooth contact and thus a high speed when gripping. This means that screw connections can be made safely, quickly and with a lot of force.
Kraftform Compact VDE extra slim – effortless screwing even when things get tight
When screwing in electrical systems, screwdrivers with conventional blades often reach their limits because they are too large. For example, the screwdriver blade must be inserted deep into the component in connection, chandelier or terminal blocks in order to reach the screw or spring elements. This is only possible with slim blades that are precisely tailored to this application.For these purposes, Wera has the “VDE Kraftform Compact Blades” in its range, which are “extra slim” and have a significantly reduced diameter compared to conventional blades. This means that even deep-set screws in electrical components made of insulating materials can be screwed reliably and securely.
Despite their slim design, high robustness and a long service life are guaranteed. The protective insulation is integrated into the blade and practically wear-free, so that frayed insulations are a thing of the past.
The extra slim blades also fit into the Kraftform handle of the Kraftform Compact System.
Kraftform Kompakt VDE Torque – for consistent quality on every screw
Force-controlled screwdriving in the range from 1.2 to 3.0 Nm is possible with the Kraftform Kompakt VDE Torque torque screwdriver from Wera, the tool manufacturer from Wuppertal.This effectively prevents damage to the screw or workpiece and ensures the safety of the screw connection. The torque can be adjusted quickly and easily via a window scale. If the selected value is reached, the user hears and feels a clear overrun.
The manual release torque of the Torque tool is unlimited. With Wera’s tried-and-tested handle/changeable blade system, the exchange and reception of insulated changeable blades can be carried out at lightning speed.
Have you ever heard of PlusMinus screws?
Wera has corresponding PlusMinus tools in all segments presented. But what is a PlusMinus screw?
PlusMinus screws have a screw head with a profile combination of cross slot and slot. Just like the classic cross-slot profile, the PlusMinus profile also distinguishes between Phillips-Recess and Po-zidriv. This is why there are two different PlusMinus screws PH/S and PZ/S, which, by the way, are particularly used for terminal blocks, fuse boxes, switches and relays.


Images: WERA