The Raspberry Pi is ideally suited to learn all technical topics in a practical way and at a reasonable cost in the private and school environment.
Its compact and open design opens up a large universe of possibilities here.
Thanks to the compatibility with modern programming languages such as Scratch and Python, the learning objectives can be ideally tailored to the relevant age group. The spectrum ranges from school beginners to students and trainees.
The new Joy-Pi-Note from Joy-iT follows a comprehensive concept
With its 29.5 cm (11.6 “) IPS screen and a removable, wireless keyboard, it adopts the basic idea of the Joy-Pi experiment case in a new, high-quality and attractive format. With 46 courses and 18 projects, the Joy-Pi Note is not only suitable as an experiment center, but is also ideal for use in the education sector. With over 22 integrated sensors and modules, there are no limits to your joy in experimenting. This simplifies entry into electrical engineering and programming.The built-in units can be operated and learned independently of your own prior knowledge thanks to the learning platform that has been specially developed for the Joy-Pi Note. It is also possible to connect additional sensors and modules via the external pins of the Raspberry Pi and thus to carry out more complex projects.
Of course, the Joy-Pi Note can also be used as a “classic” notebook. All programs compatible with the Raspberry Pi® 4 can be installed. Thanks to the integrated 2MP camera, video conferences, for example, are also possible.
On the underside of the device you will find a compartment in which you can insert a power bank to operate the Joy-Pi Note mobile.

Images: JOY-IT