Using digital twins to create a smart supply chain

Mit einem digitalen Zwilling zur smarten Supply Chain

A digital twin is a virtual representation of a physical object, process or process system. It is based on real-time data and enables in-depth analysis and predictions. In the context of logistics, a digital twin is a virtual representation of a real supply chain. Using a digital twin makes it possible to carry out comprehensive, […]

Intelligent building networking of public educational institutions

Intelligente Gebäudevernetzung öffentlicher Einrichtungen des Bildungswesens

Secure network access and reliable data transmission are particularly vital when it comes to educational institutions. An infrastructure tailored to everyday learning supports all usage scenarios, such as individual research, video conferencing and teamwork via digital platforms. The integration and management of stationary and mobile end devices—some of which come from the private sector and […]

Better control of precise movements

Mechatronik bewegt mit elektrisierenden Antriebstechnik-Komponenten:
Exakte Bewegungen besser beherrschen

Motor solutions that are faster, more accurate and more energy-efficient help with the understanding of machines and devices. This has a positive effect on their quality and longevity and has the potential to reduce their ecological footprint. Operating costs and therefore the unit costs of the manufactured products are also reduced. Fast, precise movements play […]

Artificial intelligence for all

Tensor-Koprozessoren verleihen Embedded Computing KI-Fähigkeit

Artificial intelligence (AI) applications are very well suited for pattern recognition, enabling flexible decision making, for example, for driver assistance systems in cars or for industrial applications such as quality assurance. The availability of specialised tensor coprocessors and their integration into single-board computers and Computer on Module (COM) boards enable the execution of extremely CPU-intensive […]

Lend me your arm

Maschinen durch Roboterintegration transformieren

We usually see industrial robots working as standalone complete machines. However, in recent times, there has been much talk of cobots—robots that are optimised to work with humans. No less exciting is the use of robots in conjunction with production and packaging machinery. A silver bullet is not forthcoming, instead we have three completely different […]

Developer boards in industrial applications

Entwicklerboards im industriellen Einsatz

Boasting benefits such as a compact design, low power consumption and an affordable purchase price, developer boards are suitable for a wide range of projects. They are also being increasingly used in industrial applications. Engineers now have a number of interesting development boards at their disposal for this purpose—with Arduino products coming in first. Below, […]

Closing digitalisation gaps

Requirements for consistent automation concepts: Closing digitization gaps

Over the past few years, trade and industry have invested a great deal in digitalising production processes. Nevertheless, the path to Industry 4.0 is still a long one for many companies, particularly smaller ones. It is also littered with digitalisation gaps that, like potholes in the road, slow down efficiency. Closing these gaps opens up a path towards the transformation of production processes.

Guaranteed safe functioning

Use safety sensors for "grey" and "yellow" tasks

The broader the decision-making basis in automated machines or plants for their control or higher-level systems, the more precisely the production result can be controlled. Sensors provide the basis for this, which is why more and more of them are being used. Hardware requirements can be limited by using safety-related sensors for even non-safety-related purposes. […]

How to ensure a small CO2 footprint

Der Weg zum schlanken CO2-Fußabdruck

When developing products, it is more relevant than ever to think about their environmental impact. A large number of components must be taken into account. The earlier in the process the various factors are weighed up in order to resolve the conflicts of goals with the best possible compromises, the better the overall result will be. The most effective way to do this is to plan production and its automation right from the product definition stage.

Smarter robots can do more

Smarter robots can do more

Artificial intelligence (AI) applications improve the ability of industrial robots to react quickly and precisely to sensor and image data. Integrating AI functionality directly into the robot control system enables not only accelerated object recognition, but also increases in quality, reliability and speed, as well as extending the possibilities for working with people.