‘Dashcams make drivers more careful’ say nearly of 50% of Brits

Umfrage: Großteil der Deutschen legt keinen Wert auf BGH-Urteilskonformität ihrer Dashcam

Research by OnePoll reveals that 34% of drivers say using Dashcams makes road traffic safer. While 42% of Dashcam users believe other drivers take more care on the road too. Dashcams provide added security Personal and vehicle security are prominent concerns and the main reason Brits choose to buy a Dashcam. 64% say these in-car cameras provide […]

UK companies underestimate the benefits of LED lighting

Deutsche Unternehmen unterschätzen Potential von LED

Almost half aren’t planning to switch to LED in next 12 months, despite upcoming halogen ban. British companies are failing to adequately prepare for the upcoming halogen light bulb ban in 2018, as 41 percent are choosing not to switch to the alternative LED lighting in the next 12 months. This is according to our […]

Nearly half of UK homes aren’t insured against damage caused by lightning

Stecker ziehen bei Gewitter? Nur jeder dritte Jugendliche tut es

Our new research reveals a startling 47 per cent of UK adults don’t know if they are insured against lightning damage. 26 per cent admitted to not being insured at all against over-voltage. A single lightning bolt can cost more than £45,000 worth of damage (source: Direct Line). Younger generations could find themselves paying the […]

Over half of UK adults NEVER change their WiFi password

Two thirds complain about poor WiFi

55 percent of Brits use passwords to protect their router but fail to change their WiFi password regularly. Our new research has revealed that whilst most UK adults are familiar with using router passwords to protect their WiFi (85 percent), 55 percent of users are actually putting themselves at risk by never changing their passwords, […]

A third of Brits choose LED lights to save energy

Eine repräsentative Umfrage von reichelt elektronik zeigt: An LED geht kein Weg mehr vorbei. Was den Deutschen beim Kauf von LED-Leuchtmitteln besonders wichtig ist, erfährst du hier!

LED lights have become a viable option for UK households wanting to make energy and cost savings, our recent research has revealed. Lasting significantly longer than conventional lamps, a third of respondents say energy savings are the biggest influencer when it comes to buying an LED light but upfront costs remain a barrier to purchasing. […]

Nearly 1 in 5 electrical installations in UK homes are inadequate

Umfrage Elektroinstallationen

In almost one fifth (19 percent) of UK households, there are signs of overloading of electrical installations, results from our survey show. The research also revealed that the East of the UK experienced the greatest number of electrical overloads (23 percent) when several electrical devices were used at the same time, effecting lights or causing […]

Digital photos: Put the camera away — and then what?

Digitalfotos: Aufnahme im Kasten – und dann?

The smartphone made normal cameras obsolete quite some time ago. And it’s no wonder, after all there is always a smartphone to hand. It’s quick to take a photo. But what happens with all the great memories, spectacular selfies and unique snapshots? Digital photos: Put the camera away? The following fact shows how important this […]