Rapidly produce ultra precise molds and final parts, in-house with the Mayku Multiplier

Thermoforming is the perfect choice for businesses needing to develop a prototype quickly and efficiently, as they can produce it in-house within hours, rather than days. From concept models to functional prototypes, thermoforming offers a wide range of design possibilities with high accuracy, making it fast and cost-effective. Detailed pressure former for maximum flexibility With […]
Lapp Mobility – the fuel for e-mobility!

Lapp Mobility GmbH is a corporate start-up from Lapp, the global market leader for integrated cable and connection technologies. The family-run company from Stuttgart has specialized in the development, manufacture and sale of charging systems for electric cars. Lapp Mobility is not only “Made in Germany”, but also relies on a sustainable supply chain in […]
The universal plug-in power supplies from FRIWO – now available in the reichelt shop

The electrical supply is a minimum requirement for ensuring operation. Especially for medical applications and security of supply, because the safety of patients is at stake here. It is therefore not surprising that medical facilities often have their own emergency power generator to keep the equipment running even in the event of a failure. The […]
Space-saving and robustly wired: The new VariFLEX patch cables

The employees of TTL Network GmbH are experts in development of cables. It is particularly important to them to always respond to the needs of the customers, which they have succeeded in doing again with the new VariFLEX patch cable: space-saving and at the same time very robust, the patch cables have high quality standards […]
The hybrid laser plotter from xTool

An unlimited number of design options for hobbyists, amateurs and professionals. With the new hybrid laser plotters for cutting and engraving from xTool, there are no limits to creativity. The devices combine powerful lasers with sharp knives and thus guarantee the greatest possible scope for various ideas and their implementation. The two hybrid laser plotters […]
Camping antennas with WiFi router now in 5G

The camping holiday trend is growing steadily. In order to be able to use high-speed internet while on vacation, the new 5G mobile communications standard enables data transmission up to ten times faster than its predecessor 4G and has been continuously expanded. With the new Falcon 3307 roof antenna and the Falcon 3309 window antenna, data transmission at 5G speed is now also standard on camping holidays – and also enables convenient remote working and streaming.
Protection for electronic components – with the ESD-PLA filaments from Material 4 Print

Companies and private individuals have been enthusiastic about the possibilities of 3D printing for years. If it was not yet possible to protect electronic components from unwanted voltage peaks with the previously available fillers, Material 4 Print offers a solution to this problem with its new ESD-PLA filaments. The new selection of filaments is now […]
New Revolution Pi S/SE series based on the Raspberry Pi Compute Module 4S

Mit der Revolution Pi S- und SE-Serie erweitert KUNBUS sein Programm um neue Basismodule seines Open Source IPCs, die erstmals auf dem Raspberry Pi Compute Module 4S. Die neuen Serien sind zwischen der 3+ Serie und der kommenden RevPi 4-Serie angesiedelt. Folgende Module werden als S/SE-Serie erhältlich sein: RevPi Core, RevPi Connect und RevPi Flat. […]
Brother Pro Tapes

Brother Pro Tapes are specifically designed to meet the needs of experts who require reliable, durable and long-lasting labelling solutions. Always the right tape Brother understands the importance of accurate labeling that is reliable and consistent. For this reason, we have developed various Pro Tapes for a wide variety of applications, whether for labeling cables, […]
Inspection camera for every tool bag

Inspection cameras for cavity testing in technical applications are now well-known in the industry as well as for private users. There are a large number of devices of different price and performance classes on the market, which does not exactly simplify the decision for the right inspection camera. For a short and uncomplicated entry into […]