New to the range: Round OLED displays, fast and temperature-stable

Circular, high-contrast, ultra-thin, power-saving and stable over a very wide temperature range: The OLED displays of the EA W128128-XR series are ideal for use in compact handheld devices. The dimensions The new OLED displays from ELECTRONIC ASSEMBLY are only 2.05 mm thick. Their display area has a diameter of 30 mm (1.2″) and consists of […]
Pendant lights quick, clean and easy to install: Finally gap-free!

The following situation certainly looks familiar to you: You have bought a new ceiling lamp which now needs to be installed. The bracket is attached, the plugs are connected to each other and now the canopy comes into play, which should “disappear” the ceiling plate and the whole cable spaghetti. But no matter how you […]
The new Raspberry Pi 4 is here and exceeds all expectations

Before we go into more detail about the technical innovations of the Raspberry Pi 4, we would like to briefly go into the topic of developer boards in general. Especially the brand Raspberry Pi.
Ecological and economical printing thanks to EcoTank

Today, decisions in many companies are not always made on the basis of purely economic considerations – environmental awareness is also playing an increasingly important role. A starting point for saving costs and protecting the environment is, for example, the high consumption of resources in printing.
Eufy surveillance camera – 365 days burglary protection with one battery charge

Whether in private households or public institutions – surveillance cameras are enjoying growing popularity. But even the best security camera is useless if the battery is empty. And that can happen quickly.
First intelligent language assistant for drivers

Using the mobile phone while driving is not only negligent, it is also forbidden. Nevertheless, many drivers find it difficult to keep their hands off their smartphone.
Now available at reichelt: Laser products from Picotronic

Reichelt expands its range of laser modules by a well-known manufacturer: Picotronic. 200 new products of the leading supplier of laser modules are now available in the reichelt shop.
Entry into automation – with the DOBOT Magician robot arm

The DOBOT Magician is a versatile robot arm, which is mainly used for learning programming skills. With the extension attachments such as the 3D printing set or the gripper arm, various scenarios can be tested with little effort. This makes it the ideal introduction to robotics and automation technology. Getting Started in Robotics Without Hurdles […]
Is the Rock Pi a powerful alternative to the Raspberry Pi?

The Rock Pi from Radxa is a particularly powerful single board computer for anyone planning challenging projects. What’s particularly interesting about Rock Pi is that you have several choices: Model A is the basic version with a powerful RK3399 Rockchip and Ethernet connection. Model B also includes WiFi, a Bluetooth connection and optional PoE. Both […]
Cutting, stripping, twisting and crimping with only one tool

Wiring industrial plants and control cabinets is often a laborious task, which requires permanent work with the highest accuracy and consistent quality.