With LOGO! 8.3, the popular Siemens small controller is connected to the cloud

With cloud connection for more efficiency and flexibility The new version 8.3 has a cloud connection, bringing the possibilities of a smart factory to even the most compact automation project. For example, measured values for key indicators of the condition of a machine or plant can be collected and evaluated to prevent errors as well […]
Avoid critical aerosol concentrations with Testo’s practical measuring instruments

Whenever we breathe and speak, aerosols are produced. Normally unproblematic, these can, however, also transmit pathogens and viruses. The risk of infection is much higher indoors than outdoors. Aerosols remain in the air longer, which means that the risk of unnoticed spread of pathogens is constantly increasing. It is therefore important to keep an eye […]
Smart Home via Bluetooth – Frogs as real communication talents

Turning one’s own four walls into a smart home – that is what more and more owners and tenants want. But many shy away from high costs, complicated handling and data storage in the cloud. With smart boards called Frogs, frogblue provides the solution: the Bluetooth LE-based system does without the cloud, is impressively simple […]
New resin materials for 3D printing from Formlabs

The renowned manufacturer of 3D printing systems Formlabs introduces a new product family of synthetic resins: the Flexible and Elastic Resins. Formlabs has already made a name for itself as a developer of particularly powerful and accessible systems for 3D printing. The new resin materials for desktop 3D printing are soft and easy to process, […]
New high performance LED construction spotlights by Brennenstuhl

Every do-it-yourselfer and craftsman has certainly already stood in the dark on a construction site. In the past, high-performance halogen spotlights or particularly bright solutions with HQL lamps had to provide the necessary illumination. Both options not only consume a lot of energy and possibly cause high electricity costs, but are rarely equipped with useful […]
The Leica Lino L6R & L6G line lasers

The Leica Lino L6R & L6G feature three 360° multi-line lasers with excellent visibility. The instruments from Leica Geosystems are quick and easy to set up and can be positioned precisely with their magnetic adapters. The Lino L6R is available with red and green lasers and in different configurations. What makes the instruments stand out: […]
The Smart Home Bridge from Rademacher makes it easy to create a networked home

If you want to set up a smart home, you have to think a lot at the beginning: What about security? What must the future system be compatible with? And what extensions will be added in the future? The new Smart Home Gateway from Rademacher puts an end to these headaches. Because it allows users […]
Varta Energy Powerbanks: Powerful and safe energy sources on the move

Anyone who has ever run out of battery power from a mobile phone or camera at the crucial moment knows how valuable a powerbank can be. It can be used to supply small appliances with new energy even when on the move. reichelt elektronik has recently launched the powerbanks of the Energy series from Varta […]
Ready for use at any time with high user comfort: Tool case set XXL III from Wiha

Physical work on building sites is demanding. It becomes even more strenuous when heavy tools have to be carried around. This is where the new tool case XXL III electric from Wiha provides relief and comfort. It is specially designed to meet the requirements of mobile use under difficult conditions. It can be conveniently transported […]
Smart home in next to no time with the Homematic IP WLAN Access Point

Safe, uncomplicated and visually unobtrusive: that’s how most users want their smart home. To get even closer to this idea, Homematic IP has developed a new WLAN access point. We explain what the product can do. Easy to set up and offering a wide range of options As the control centre for the intelligent devices, […]