Fischer EasyHook: Turn the screw into a hook

Conventional screw hooks are used in almost every wall. Whether it’s to attach shelves, signs or decorative objects to the wall – almost everyone has already inserted a screw hook into a wall. However, with such conventional hooks, unsightly effects or even damage can occur already during the screwing process but also later during use: […]

ESD toggle clamps make it easier to manufacture and assemble electronic devices

In production systems, partially or fully automated production lines, small series development and final assembly always have one thing in common: As soon as parts or assemblies can move too much, manufacturing errors can often not be ruled out. It does not matter whether, for example, unwanted vibrations occur on the system itself or the […]

For maximum safety: UL-certified wire-end ferrules from Vogt AG

The quality wire-end ferrules produced millions of times in Switzerland by Vogt AG Verbindungstechnik have been awarded the globally recognised UL safety test mark. Vogt’s wide range of UL ferrules covers cable cross-sections from 0.5 mm2 to 50 mm2 (AWG 20-1/0) and offers different ferrule lengths with matching certified crimping tools. The ferrules are tested […]

Chia Mining – is the hype causing a hard drive shortage?

The new, more energy-saving crypto currency Chia triggered a real hype even before its launch. But if you want to be part of Chia Mining, you have to be quick, because the hard drives required for this are becoming scarce and their prices are rising rapidly. What is chia mining and why does it make […]

KUNBUS GmbH: Raspberry Pi-based IoT gateway for the energy industry

Intelligentes Energiemanagement mit dem RevPi Flat

The RevPi Flat is the latest member of the Revolution Pi family from KUNBUS. At first glance, its untypical design stands out, which is clearly different from the well-known RevPi Core and RevPi Connect modules and is more reminiscent of the RevPi Compact. This design was deliberately chosen so that the module can be easily […]

From PET bottles to the laptop cases – DICOTA focuses on sustainability

Sustainability through recycling: DICOTA shows how it works. In order to increase the proportion of plastic waste, the Swiss company uses up to 12 PET bottles to produce laptop cases or tablet sleeves. This ensures lower consumption of raw materials as well as energy. reichelt elektronik has a diverse selection of bags and cases from […]

The end of OSRAM Lightify?

Before the end of this year, on 21.08.2021, Osram will discontinue the cloud-based server operation and support of Lightify. The system, with which OSRAM competed against its counterpart Hue from Philips, is getting on in years and technically outdated. There will be no more updates and the cloud-based use of the voice assistants Google Assistant […]

Laxihub: The new generation of intelligent surveillance cameras

Those who want to equip their homes with smart technology today are increasingly turning to smart surveillance cameras. With their sophisticated technology, they offer users protection for their own homes. reichelt elektronik offers WiFi-enabled cameras for indoor and outdoor use as well as the smart video doorbell from Laxihub. Wireless technology from the Netherlands – […]