Smart home with thread – this technology is set to become the new standard

Fast, reliable smart home technology that is compatible with all manufacturers and easy to install – that’s what we want for our intelligent home. This is possible with the innovative thread technology! The new standard is a quantum leap for smart home development. Thread technology is already built into Eve products and the HomePod mini. […]
Ready for the camping season: More comfort with the right technical equipment

For enthusiastic campers, the anticipation of the next holiday starts with preparing the camper van. You can do this at any time and get a bit of a holiday mood. What is definitely worthwhile is to put the technical equipment of the camper to the test again. Whether it’s navigation systems or power banks for […]
Bring light into the dark – what you need to know for the correct use of infrared spotlights

Infrared spotlights are valuable tools to improve the quality of video surveillance recordings at night. In this guide you will learn how you can equip surveillance cameras with additional infrared emitters and what you need to know for correct use. Advantages of infrared headlights Night recordings with digital surveillance cameras generally require external light sources. […]
Extreme types: Adhesives for special conditions
Have you ever heard of adhesives for temperatures far above 100 degrees, for humid environments, even for adhesion under water? If not, that’s about to change. We introduce you to a few “super adhesives” that withstand extreme conditions. What matters when choosing an adhesive Gluing is a great thing. No time-consuming drilling, screwing, riveting or […]
Why switch from “good” leaded solders to lead-free solders when soldering by hand?

Electronics manufacturers have stipulated that they must use lead-free solders for the manufacture of their assemblies. According to this law, “lead-free” means solders that do not contain more than 0.1% lead and are therefore below the specified limit values. This EU directive was replaced by 2011/65 / EU in 2013. Nothing has changed in the […]
Wait, just a second! Interesting facts about instant adhesives
When something needs to be glued quickly, we like to use the well-known instant glue. As the name suggests, it bonds almost all materials to and with each other in a flash. These include, for example, metal, plastic, glass, ceramics, wood, leather or rubber. But how does the very fast reaction time of the adhesive […]
New EU drone regulation – what needs to be considered

Nowadays, drones are used in a variety of sizes and configurations as well as in different application scenarios. They are used privately, for example, to make film recordings from a bird’s eye view or simply to have fun with technology. But even in professional use, drones can be used in a variety of ways and […]
AMD chipsets in check

The chipset has a great influence on the overall performance of the computer system because, as the central element on the motherboard, it controls the flow of data between the processor, main memory, bus systems and the controllers of the internal and external interfaces. The choice of the right chipset determines which components can be […]
Intel Chipsets in check

The chipset is the central element on a motherboard and acts as a link between the individual components of a computer. It controls the interaction and the flow of data between the processor, the main memory, the bus systems and the controllers of the internal and external interfaces and therefore has a major influence on the overall performance of the computer system. Choosing the right chipset is important because it determines what components can be used in a computer system.
If you now look at the composition of an Intel-based desktop PC, you need to select the right mainboard and the chipset, which contains all the components of the PC, such as RAM, SSD, graphics adapter and the CPU, which is mounted on a socket. The CPU socket and the chipset of the mainboard must match the respective CPU.
Window ventilation, secondary air units and co – Proper ventilation at home and in the office

Whether at home or at work, when it gets cold outside, the windows are opened less often for reasons of comfort. Adequate ventilation is important in all seasons – perhaps even most important in winter, when infections spread faster. Viruses and bacteria can be spread by droplets and aerosols. As the droplets sink to the […]