ZOTAC’s all-new ZBOX C Series brings a new light to the computing experience  

ZOTAC’s all-new ZBOX C Series brings a new light to the computing experience

ZOTAC has completely redesigned and further developed its Z-BOX C Series. The hardware in this series is even stronger than before and the timeless, stylish design has even been awarded the Computex d & i Award. The biggest highlight, however, is the completely silent operation.

Strong. Quiet. Fast. Clear.

The ZBOX C-Series is quiet, strong and fast. The cooling performance has increased by 66 percent compared to the previous generatio and the passive cooling hardware processes up to 25W TDP processors.

Due to the lack of moving parts, the PCs‘ life is extended and helps to ensure complete silence. The innovative design features a 90 percent ventilated surface, ensuring 270-degree breathability. Based on nature’s extremely resilient honeycomb structure, all C series mini PCs have a maximum air-permeable surface.

On this inside, the Intel® Core ™ i7 processor of the 8th generation ensures maximum speed. It‘s four cores and Hyperthreading ™ delivers top performance and with HDMI 2.0 and DisplayPort 1.2, the new ZBOX C series is dual-display ready. The integrated Intel UHD Graphics 620 enables 4K at 60Hz resolution in addition to the H.265 / HEVC Main10 profile for crisp, clear images.

Versatile design combined with power

The small, powerful and quiet ZBOX C Series is also extremely agile. No matter how or where the mini PC is to be placed, hung on the wall or hidden behind a monitor, thanks to the compact 204mm x 129mm x 68mm dimensions, there are no limits. And if access to the SO-DIMM memory slots or the 2.5-inch HDD / SSD bay should be required, it is, as with all ZOTAC ZBOX mini-PCs, also possible in the C-series without using any tools.

Cover picture: Manufacturer

 

What do you think about this topic? Leave a reply:

Your email address will not be published. Required fields are marked *