0
  • Shopping cart
  •  €0.00
  • Shipping costs
  •  €from 5.60
CatalogueRNDRaspberryreichelt Magazin

See what our German
customers think:


Verified Service

We offer you the highest level of trust and security.

reichelt certificate

reichelt elektronik GmbH & Co. KG
Elektronikring 1
26452 Sande Germany

phone: +49 (0)4422 955-333
mail: info@reichelt.de
www.reichelt.de


Raspberry Pi - the compact all-rounder

Since it was launched at the beginning of 2012, millions of Raspberry Pi computers have been sold, making it the world’s most popular single-board computer. The applications are so diverse that many Raspberry Pi users have more than one of theses computers in their home.

For example, the compact all-rounder can be used as an HD media player with an external hard drive for home cinema or as an Internet radio with a display. It can also be used as a webcam server for livestream camera monitoring to a smartphone and for home automation such as controlling the heating and lights, or as a simple WLAN print server or as a mini-computer for general surfing on the Internet.

As you can see, this amazing little computer is not only versatile, but is also extremely inexpensive, which is what makes it so attractive. In principle, you do not even need any programming skills, due to the wealth of programming instructions offered in forums and books, or you can simply install a complete image on the Raspberry Pi and you are ready to go! Don´t be afraid to try!
Raspberry Pi Bundles

More than 250 accessory products from
A as in Adapter to Z as in Zigbee

In our hand-picked product assortment you will find everything you need for your future Raspberry Pi project. From LCDs, cameras, UPS units or expansion boards to sensors, such as temperature, acceleration, gas or humidity sensors, as well as enclosures, high-quality sound cards, relay controllers or interfaces such as Bluetooth, WiFi, NFC and RFID. But there is also much more, and at excellent prices, from well-known manufacturers such as Raspberry Pi, Adafruit, HiFiBerry, Joy-IT, Seeed, Max2Play, Pi-Top, etc.
Raspberry Pi 3 A+, 4x 1,4 GHz, 512 MB RAM, WLAN, BT

Discover the reichelt magazine

Information and inspiration for novices, advanced users and experts. Discover technology news, exciting projects and take advantage of our guides & how-to articles.

  • 100% portable use - always up to date, also with a tablet or smart phone
  • 100% free - all information available immediately, no subscription, no registration
  • 100% reichelt - no banner advertising, manufacturer-independent - the best of everything

Discover what is possible with the Raspberry Pi

With our how-to articles about single-board computers, especially the Raspberry Pi, you will quickly discover the endless possibilities offered by this little powerhouse.
For example:

  • Turn your home into a smart home with the Raspberry Pi
  • Getting started
  • Adblocker for the entire network, thanks to Raspberry Pi
  • Experience real retrogaming with RPi and RetroPi in the NESPi case.

and much more!

Our manufacturers at a glance

reichelt printfooter